public interface WaitNodeConfigFactory
| Modifier and Type | Method and Description |
|---|---|
AnalogInputCurrentWaitNodeConfig |
createAnalogInputCurrentConfig(AnalogIO input,
CompareOperator compareOperator,
Current current,
ErrorHandler<Current> errorHandler)
Creates a configuration for waiting for an analog input to go past an electric current threshold.
|
AnalogInputVoltageWaitNodeConfig |
createAnalogInputVoltageConfig(AnalogIO input,
CompareOperator compareOperator,
Voltage voltage,
ErrorHandler<Voltage> errorHandler)
Creates a configuration for waiting for an analog input to go past a voltage threshold.
|
DigitalInputWaitNodeConfig |
createDigitalInputConfig(BooleanRegister input,
boolean valueToWaitFor)
Creates a configuration for waiting for a boolean register to go
true or false. |
DigitalInputWaitNodeConfig |
createDigitalInputConfig(DigitalIO input,
boolean valueToWaitFor)
Creates a configuration for waiting for a digital input to go high or low.
|
DigitalInputWaitNodeConfig |
createDigitalInputConfig(ModbusIO input,
boolean valueToWaitFor)
Creates a configuration for waiting for a digital MODBUS input to go high or low.
|
ExpressionInputWaitNodeConfig |
createExpressionInputConfig(Expression expression)
Create a configuration for waiting for an expression to be evaluated to true.
|
FloatRegisterInputWaitNodeConfig |
createFloatRegisterInputConfig(FloatRegister input,
CompareOperator compareOperator,
float valueToWaitFor)
Creates a configuration for waiting for a register to go past a float threshold.
|
TimeWaitNodeConfig |
createTimeConfig(Time time,
ErrorHandler<Time> errorHandler)
Creates a configuration for waiting a specified amount of time.
|
TimeWaitNodeConfig createTimeConfig(Time time, ErrorHandler<Time> errorHandler)
time - the time to wait, not null.errorHandler - handler for validation errors. If using ErrorHandler.AUTO_CORRECT
this will clamp the value to the nearest valid time value.DigitalInputWaitNodeConfig createDigitalInputConfig(DigitalIO input, boolean valueToWaitFor)
input - the digital input on which to wait, not null.valueToWaitFor - true, if waiting for the input signal value/level to go HIGH, false
otherwise (waiting for LOW signal value/level).IllegalArgumentException - if input is an output (does not support reading of values).
See IO.isInput().DigitalInputWaitNodeConfig createDigitalInputConfig(ModbusIO input, boolean valueToWaitFor)
input - the digital MODBUS input on which to wait, not null.valueToWaitFor - true, if waiting for the input signal value/level to go HIGH, false
otherwise (waiting for LOW signal value/level).IllegalArgumentException - if input is an output (does not support reading of values)
or if output is not a digital output. See IO.isInput() and IO.getType().DigitalInputWaitNodeConfig createDigitalInputConfig(BooleanRegister input, boolean valueToWaitFor)
true or false.input - the boolean register input on which to wait, not null.valueToWaitFor - true, if waiting for the register to be true, false otherwise.IllegalArgumentException - if input is an output (does not support reading of values). See IO.isInput().AnalogInputCurrentWaitNodeConfig createAnalogInputCurrentConfig(AnalogIO input, CompareOperator compareOperator, Current current, ErrorHandler<Current> errorHandler)
input - on which to wait, not null.compareOperator - the operator to use when comparing input to value, not null. Available options are
"less than" (<) or "greater than" (>).current - the electric current threshold to wait for, not null.errorHandler - the error handler for validation errors. If using ErrorHandler.AUTO_CORRECT
this will clamp the value to the nearest valid current value.IllegalArgumentException - if input is an output (does not support reading of values). See IO.isInput().AnalogInputVoltageWaitNodeConfig createAnalogInputVoltageConfig(AnalogIO input, CompareOperator compareOperator, Voltage voltage, ErrorHandler<Voltage> errorHandler)
input - on which to wait, not null.compareOperator - the operator to use when comparing input to value, not null. Available options are
"less than" (<) or "greater than" (>).voltage - the voltage threshold to wait for, not null.errorHandler - the error handler for validation errors. If using ErrorHandler.AUTO_CORRECT
this will clamp the value to the nearest valid voltage value.IllegalArgumentException - if input is an output (does not support reading of values). See IO.isInput().FloatRegisterInputWaitNodeConfig createFloatRegisterInputConfig(FloatRegister input, CompareOperator compareOperator, float valueToWaitFor)
input - the float register input on which to wait, not null.compareOperator - the operator to use when comparing register to value, not null. Available options
are "less than" (<) or "greater than" (>).valueToWaitFor - the float threshold to wait for.IllegalArgumentException - if input is an output (does not support reading of values). See IO.isInput().ExpressionInputWaitNodeConfig createExpressionInputConfig(Expression expression)
expression - the expression to evaluate, not null.Copyright © 2019. All rights reserved.