public interface SetNodeConfigFactory
| Modifier and Type | Method and Description |
|---|---|
AnalogOutputCurrentSetNodeConfig |
createAnalogOutputCurrentConfig(AnalogIO output,
Current current,
ErrorHandler<Current> errorHandler)
Creates an analog output current configuration.
|
AnalogOutputVoltageSetNodeConfig |
createAnalogOutputVoltageConfig(AnalogIO output,
Voltage voltage,
ErrorHandler<Voltage> errorHandler)
Creates an analog output voltage configuration.
|
DigitalOutputSetNodeConfig |
createDigitalOutputConfig(BooleanRegister output,
boolean valueToSet)
Creates a digital output configuration.
|
DigitalOutputSetNodeConfig |
createDigitalOutputConfig(DigitalIO output,
boolean valueToSet)
Creates a digital output configuration.
|
DigitalOutputSetNodeConfig |
createDigitalOutputConfig(ModbusIO output,
boolean valueToSet)
Creates a digital MODBUS output configuration.
|
ExpressionOutputSetNodeConfig |
createExpressionOutputConfig(IO output,
Expression expression)
Create an expression output configuration.
|
FloatRegisterOutputSetNodeConfig |
createFloatRegisterOutputConfig(FloatRegister output,
float valueToSet)
Create a float register output configuration.
|
SingleDigitalPulseSetNodeConfig |
createSingleDigitalPulseConfig(BooleanRegister output,
Time pulseTime,
ErrorHandler<Time> errorHandler)
Creates a single digital pulse configuration.
|
SingleDigitalPulseSetNodeConfig |
createSingleDigitalPulseConfig(DigitalIO output,
Time pulseTime,
ErrorHandler<Time> errorHandler)
Creates a single digital pulse configuration.
|
SingleDigitalPulseSetNodeConfig |
createSingleDigitalPulseConfig(ModbusIO output,
Time pulseTime,
ErrorHandler<Time> errorHandler)
Creates a single digital pulse MODBUS configuration.
|
DigitalOutputSetNodeConfig createDigitalOutputConfig(DigitalIO output, boolean valueToSet)
output - the digital output to apply the output action to, not null.valueToSet - if true the output will be set to HIGH, otherwise LOW.IllegalArgumentException - if output is an input (does not support writing of values). See IO.isInput().DigitalOutputSetNodeConfig createDigitalOutputConfig(ModbusIO output, boolean valueToSet)
output - the digital MODBUS output to apply the output action to, not null.valueToSet - if true the MODBUS output will be set to HIGH, otherwise LOW.IllegalArgumentException - if output is an input (does not support writing of values)
or if output is not a digital output. See IO.isInput() and IO.getType() .DigitalOutputSetNodeConfig createDigitalOutputConfig(BooleanRegister output, boolean valueToSet)
output - the the boolean register output to apply the output action to, not null.valueToSet - the value to apply to the output register.IllegalArgumentException - if output is an input (does not support writing of values). See IO.isInput().AnalogOutputCurrentSetNodeConfig createAnalogOutputCurrentConfig(AnalogIO output, Current current, ErrorHandler<Current> errorHandler)
output - the analog output to apply the output action to. The output should be configured to use electric
current domain, not null.current - the electric current value/level to set, not null.errorHandler - error handler for handling validation or domain (i.e. current or voltage) errors. If using
ErrorHandler.AUTO_CORRECT this will clamp the value, and in case of domain error, set
the value regardless of the output's domain type.IllegalArgumentException - if output is an input (does not support writing of values). See IO.isInput().AnalogOutputVoltageSetNodeConfig createAnalogOutputVoltageConfig(AnalogIO output, Voltage voltage, ErrorHandler<Voltage> errorHandler)
output - the analog output to apply the output action to. The output should be configured to use voltage
domain, not null.voltage - the voltage value/level to set, not null.errorHandler - error handler for handling validation or domain (i.e. current or voltage) errors. If using
ErrorHandler.AUTO_CORRECT this will clamp the value, and in case of domain error, set
the value regardless of the output's domain type.IllegalArgumentException - if output is an input (does not support writing of values). See IO.isInput().FloatRegisterOutputSetNodeConfig createFloatRegisterOutputConfig(FloatRegister output, float valueToSet)
output - the register to apply the value to, not null.valueToSet - the value to be set.IllegalArgumentException - if output is an input (does not support writing of values). See IO.isInput().ExpressionOutputSetNodeConfig createExpressionOutputConfig(IO output, Expression expression)
output - the output to set to the result of the evaluation of the expression, not null.expression - the expression whose evaluation will be set on the output, not null.IllegalArgumentException - if output is an input (does not support writing of values). See IO.isInput().SingleDigitalPulseSetNodeConfig createSingleDigitalPulseConfig(DigitalIO output, Time pulseTime, ErrorHandler<Time> errorHandler)
output - the digital output to apply the output action to, not null.pulseTime - the time to pulse the pin for.errorHandler - error handler for handling validation errors. If using ErrorHandler.AUTO_CORRECT
this will default the value to 0.5 seconds.IllegalArgumentException - if output is an input (does not support writing of values). See IO.isInput().SingleDigitalPulseSetNodeConfig createSingleDigitalPulseConfig(ModbusIO output, Time pulseTime, ErrorHandler<Time> errorHandler)
output - the digital MODBUS output to apply the output action to, not null.pulseTime - the time to pulse the pin for.errorHandler - error handler for handling validation errors. If using ErrorHandler.AUTO_CORRECT
this will default the value to 0.5 seconds.IllegalArgumentException - if output is an input (does not support writing of values)
or if output is not a digital output. See IO.isInput() and IO.getType() .SingleDigitalPulseSetNodeConfig createSingleDigitalPulseConfig(BooleanRegister output, Time pulseTime, ErrorHandler<Time> errorHandler)
output - the the boolean register output to apply the output action to, not null.pulseTime - the time to pulse the pin for.errorHandler - error handler for handling validation errors. If using ErrorHandler.AUTO_CORRECT
this will default the value to 0.5 seconds.IllegalArgumentException - if output is an input (does not support writing of values). See IO.isInput().Copyright © 2019. All rights reserved.