public interface FeatureContributionModel
This interface provides functionality for adding, updating and removing features in PolyScope.
Note: This interface must only be used in an installation contribution.| Modifier and Type | Method and Description |
|---|---|
Feature |
addFeature(String idKey,
String suggestedName,
Pose pose)
Add a feature to the current PolyScope installation.
|
Feature |
getFeature(String idKey)
Returns the feature previously added by this URCap using the same
idKey identifier. |
void |
removeFeature(String idKey)
Remove a feature added by this URCap from PolyScope.
|
void |
updateFeature(String idKey,
Pose newPose)
Update the pose of an existing feature added by this URCap.
|
Feature addFeature(String idKey, String suggestedName, Pose pose)
idKey - The key to identify this feature by. The key is for this URCap only, i.e. it only has to be unique for
this URCap and not "globally" for other URCaps.suggestedName - Suggested name for the feature. Valid names must match regex [a-zA-Z][a-zA-Z0-9_]{0,14} for a
total of 15 characters. The final name can be retrieved from the returned feature instance.pose - The pose of the feature with respect to the robot baseFeatureAlreadyAddedException - If a feature has previously been added the same idKey identifier.
Use getFeature(String) to check if the feature has already been added to the
current installation.
Use updateFeature(String, Pose) to update the feature.IllegalFeatureNameException - If the suggested name does not match required regex.Feature getFeature(String idKey)
idKey identifier. Use this to verify if
the feature is present in the current installation.idKey - The key to identify this feature by.null if no feature exists in the current installation.void updateFeature(String idKey, Pose newPose)
idKey - The key to identify the feature. A feature must have been added prior to this method call using the
same key.newPose - The new pose to set for the feature.FeatureNotFoundException - If no feature exists with the provided idKey.void removeFeature(String idKey)
idKey - The key used to add the feature with.FeatureNotFoundException - If no feature exists with the provided idKey.Copyright © 2019. All rights reserved.