T - The (generic) type parameter for the interface representing the type of input data entered or selected by
the end user. Relevant types are, e.g. Integer and Double.public interface UserInput<T>
| Modifier and Type | Method and Description |
|---|---|
T |
getValue() |
void |
setValueChangedListener(ValueChangedListener<T> listener)
Set a listener callback to be notified when the end user changes the associated value as well as when a new
installation is loaded or created.
|
T getValue()
CannotAccessDeprecatedUserInput - if the user input has been deprecated (using the
CustomUserInputConfiguration.deprecateUserInput(UserInput)) method)void setValueChangedListener(ValueChangedListener<T> listener)
listener - the listener callbackCopyright © 2019. All rights reserved.