public interface TCPConfiguration
With this interface, it it possible to add a TCP for a device to PolyScope as well as update the TCP's offset and remove the TCP again.
| Modifier and Type | Method and Description |
|---|---|
void |
removeTCP()
Remove the TCP of the device.
|
void |
setTCP(String tcpName,
Pose tcpPose)
Add a TCP for the device to PolyScope.
|
void |
updateTCP(Pose tcpPose)
Update the offset of the device's TCP.
|
void setTCP(String tcpName, Pose tcpPose)
Add a TCP for the device to PolyScope.
There can only exist one TCP for the device. If a TCP has already been defined, it will be overwritten with the new TCP.tcpName - The name of the TCP for the devicetcpPose - A pose for the offset of the TCP with respect to the tool output flangevoid updateTCP(Pose tcpPose)
tcpPose - The pose for the new offset to set for the TCP with respect to the tool output flange.void removeTCP()
Copyright © 2019. All rights reserved.