- All Superinterfaces:
 
- GlobalVariable, PersistedVariable, Variable
 
public interface ValuePersistedVariable
extends PersistedVariable
VALUE_PERSISTED means that the variable is stored with the installation.
 These variables are defined in the installation and will
 retain their values even when a robot is turned off and on.