public static enum AnalogOutputSelection.SelectionType extends Enum<AnalogOutputSelection.SelectionType>
Enum Constant and Description |
---|
ANALOG_OUTPUT
Analog output is selected.
|
NO_ANALOG_OUTPUT
No analog output is selected
|
Modifier and Type | Method and Description |
---|---|
static AnalogOutputSelection.SelectionType |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static AnalogOutputSelection.SelectionType[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final AnalogOutputSelection.SelectionType NO_ANALOG_OUTPUT
public static final AnalogOutputSelection.SelectionType ANALOG_OUTPUT
AnalogOutput
public static AnalogOutputSelection.SelectionType[] values()
for (AnalogOutputSelection.SelectionType c : AnalogOutputSelection.SelectionType.values()) System.out.println(c);
public static AnalogOutputSelection.SelectionType valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2019. All rights reserved.