public static enum LoopNodeConfig.ConfigType extends Enum<LoopNodeConfig.ConfigType>
Enum Constant and Description |
---|
ALWAYS
Looping infinitely has been selected.
|
COUNTER
Looping a certain number of times has been selected.
|
EXPRESSION
Looping as long as the evaluation of an expression is true has been selected.
|
Modifier and Type | Method and Description |
---|---|
static LoopNodeConfig.ConfigType |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static LoopNodeConfig.ConfigType[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final LoopNodeConfig.ConfigType ALWAYS
AlwaysLoopNodeConfig
public static final LoopNodeConfig.ConfigType COUNTER
CounterLoopNodeConfig
public static final LoopNodeConfig.ConfigType EXPRESSION
ExpressionLoopNodeConfig
public static LoopNodeConfig.ConfigType[] values()
for (LoopNodeConfig.ConfigType c : LoopNodeConfig.ConfigType.values()) System.out.println(c);
public static LoopNodeConfig.ConfigType valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2019. All rights reserved.