public static enum ForceNodeConfig.ConfigType extends Enum<ForceNodeConfig.ConfigType>
Enum Constant and Description |
---|
FRAME
Frame type is selected.
|
MOTION
Motion type is selected.
|
POINT
Point type is selected.
|
SIMPLE
Simple type is selected.
|
Modifier and Type | Method and Description |
---|---|
static ForceNodeConfig.ConfigType |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static ForceNodeConfig.ConfigType[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final ForceNodeConfig.ConfigType SIMPLE
public static final ForceNodeConfig.ConfigType FRAME
FrameForceNodeConfig
.public static final ForceNodeConfig.ConfigType POINT
public static final ForceNodeConfig.ConfigType MOTION
public static ForceNodeConfig.ConfigType[] values()
for (ForceNodeConfig.ConfigType c : ForceNodeConfig.ConfigType.values()) System.out.println(c);
public static ForceNodeConfig.ConfigType valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2019. All rights reserved.