public static enum DirectionSelection.SelectionType extends Enum<DirectionSelection.SelectionType>
Enum Constant and Description |
---|
AXIS
Direction is specified using an Axis.
|
EXPRESSION
A direction vector is specified using an Expression.
|
Modifier and Type | Method and Description |
---|---|
static DirectionSelection.SelectionType |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static DirectionSelection.SelectionType[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final DirectionSelection.SelectionType EXPRESSION
DirectionVectorExpression
public static final DirectionSelection.SelectionType AXIS
DirectionAxis
public static DirectionSelection.SelectionType[] values()
for (DirectionSelection.SelectionType c : DirectionSelection.SelectionType.values()) System.out.println(c);
public static DirectionSelection.SelectionType valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2019. All rights reserved.