public interface SwingToolbarService
| Modifier and Type | Method and Description | 
|---|---|
void | 
configureContribution(ToolbarConfiguration configuration)
This method is called once after the SwingToolbarService is registered. 
 | 
SwingToolbarContribution | 
createToolbar(ToolbarContext context)
Creates a new toolbar instance. 
 | 
Icon | 
getIcon()  | 
Icon getIcon()
NullPointerException - in case this methods returns nullvoid configureContribution(ToolbarConfiguration configuration)
The values of the ToolbarConfiguration object will be read once immediately after this method call. Changing values at a later stage will have no effect, so do not store a reference to the configuration object.
If the default values are appropriate, leave this method empty.configuration - a modifiable ToolbarConfiguration with default valuesSwingToolbarContribution createToolbar(ToolbarContext context)
context - Provides access to services and APIs relevant for the toolbarCopyright © 2019. All rights reserved.