public interface ProgramNodeServiceConfigurable
ProgramNodeService interface. If an implementation of
 ProgramNodeService also implements the ProgramNodeServiceConfigurable interface, additional properties
 for the program node contribution can be configured.
 NOTE: This interface is only relevant to URCap program nodes with a HTML-based user interface
| Modifier and Type | Method and Description | 
|---|---|
void | 
configureContribution(ProgramNodeConfiguration configuration)
This method is called once after the ProgramNodeService is registered. 
 | 
void configureContribution(ProgramNodeConfiguration configuration)
The values of the ProgramNodeConfiguration object will be read once immediately after this method call. Changing values at a later stage will have no effect, so do not store a reference to the configuration object.
If the default values are appropriate, leave this method empty.configuration - A modifiable ProgramNodeConfiguration object with default valuesCopyright © 2019. All rights reserved.