public static enum DaemonContribution.State extends Enum<DaemonContribution.State>
| Enum Constant and Description | 
|---|
ERROR
The daemon should be running but it is not 
 | 
RUNNING
The daemon is running 
 | 
STOPPED
The daemon is stopped 
 | 
| Modifier and Type | Method and Description | 
|---|---|
static DaemonContribution.State | 
valueOf(String name)
Returns the enum constant of this type with the specified name. 
 | 
static DaemonContribution.State[] | 
values()
Returns an array containing the constants of this enum type, in
the order they are declared. 
 | 
public static final DaemonContribution.State RUNNING
public static final DaemonContribution.State STOPPED
public static final DaemonContribution.State ERROR
public static DaemonContribution.State[] values()
for (DaemonContribution.State c : DaemonContribution.State.values()) System.out.println(c);
public static DaemonContribution.State valueOf(String name)
name - the name of the enum constant to be returned.IllegalArgumentException - if this enum type has no constant with the specified nameNullPointerException - if the argument is nullCopyright © 2019. All rights reserved.