public interface VariableModel
Provides methods that returns the variables that currently are registered in the system. A variable is registered if it has been stored in a DataModel instance or used for the configuration of a built-in PolyScope program node.
| Modifier and Type | Method and Description |
|---|---|
Collection<Variable> |
get(Filter<Variable> filter)
Get a subset of all the variables registered in the system using a filter.
|
Collection<Variable> |
getAll() |
FeatureVariable |
getFeatureVariable(Feature feature)
Get the feature variable for a
Feature |
VariableFactory |
getVariableFactory() |
Collection<Variable> getAll()
Collection<Variable> get(Filter<Variable> filter)
filter - see VariableFilterFactory for examplesVariableFactory getVariableFactory()
VariableFactory to create variable objectsFeatureVariable getFeatureVariable(Feature feature)
Featurefeature - the feature with a variableIllegalArgumentException - If feature not is present in the installation
or feature has no variable, see Feature.isVariable()Copyright © 2018. All rights reserved.