public interface Rotation
| Modifier and Type | Method and Description |
|---|---|
boolean |
epsilonEquals(Rotation other,
double epsilon,
Angle.Unit unit)
Indicates whether some other
Rotation object is "approximately equal" to this one. |
boolean |
equals(Object obj)
Indicates whether some other
Rotation object is "equal to" this one. |
double |
getRX()
Deprecated.
Use
getRX(Angle.Unit) instead. |
double |
getRX(Angle.Unit unit)
Provides the value of the Rx parameter in specified units.
|
double |
getRY()
Deprecated.
Use
getRY(Angle.Unit) instead. |
double |
getRY(Angle.Unit unit)
Provides the Ry parameter value in specified units.
|
double |
getRZ()
Deprecated.
Use
getRZ(Angle.Unit) instead. |
double |
getRZ(Angle.Unit unit)
Provides the Rz parameter value in specified units.
|
int |
hashCode() |
String |
toString() |
@Deprecated double getRX()
getRX(Angle.Unit) instead.@Deprecated double getRY()
getRY(Angle.Unit) instead.@Deprecated double getRZ()
getRZ(Angle.Unit) instead.double getRX(Angle.Unit unit)
unit - the unit type.double value in specified units.double getRY(Angle.Unit unit)
unit - the unit type.double getRZ(Angle.Unit unit)
unit - the unit type.double value in specified units.boolean epsilonEquals(Rotation other, double epsilon, Angle.Unit unit)
Rotation object is "approximately equal" to this one.other - another Rotation object.epsilon - a tolerance.unit - the unit type of the epsilon tolerance.true if the value of this object is "approximately equal" to the value of the other
argument; false otherwise.int hashCode()
boolean equals(Object obj)
Rotation object is "equal to" this one.Copyright © 2020. All rights reserved.