public interface JointPositionFactory
| Modifier and Type | Method and Description |
|---|---|
JointPositions |
createJointPositions(double base,
double shoulder,
double elbow,
double wrist1,
double wrist2,
double wrist3,
Angle.Unit unit)
Creates a
JointPositions object with six revolute joints using the provided angles and unit type. |
JointPositions createJointPositions(double base, double shoulder, double elbow, double wrist1, double wrist2, double wrist3, Angle.Unit unit)
JointPositions object with six revolute joints using the provided angles and unit type.base - Base joint position.shoulder - Shoulder joint position.elbow - Elbow joint position.wrist1 - Wrist1 joint position.wrist2 - Wrist2 joint position.wrist3 - Wrist3 joint position.unit - the unit type for all the joint position arguments.JointPositions object.Copyright © 2020. All rights reserved.